Rename a Data Attribute Enumerated Set

You can rename a data attribute enumerated set if needed.

Procedure

  1. Access Configuration Hub.
  2. In the NAVIGATION section, under the Configuration Hub plugin for Historian, select Tags.
  3. Select , and then select Manage Enumerated Sets.
    The Manage Enumerated Sets: <system name> window appears.
  4. Select the data attribute enumerated set that you need to rename.
    Details corresponding to the selected data set are displayed.
  5. In SET NAME, rename the name of the set.
  6. Select Save Set.
    The set name is updated.
  7. Click Done.
    The changes are saved.