Assign an Enumerated Set to a Tag
Before you begin
- Create the tag for which you want to use an enumerated set.
- Create the enumerated set that you want to assign to a tag.
About this task
Example of an Enumerated Set
Suppose you have created the
following states in an enumerated set:
Suppose you assign the enumerated set to a tag. If the tag values are, say,
50, 100, 75, and 104, when you retrieve the tag values, ON, ON, ON, and OFF,
respectively, are retrieved instead of the actual tag values.
State Name | State Range |
---|---|
ON | 0 to 100 |
OFF | 101 to 200 |
Procedure
- Access Configuration Hub.
- In the NAVIGATION section, under the Configuration Hub plugin for Historian, select Tags.
-
Select the tag to which you want to assign an enumerated set.
The details of the tag appear in the DETAILS section.
-
Under Collection, select Enumerated
Set.
-
In the upper-left corner of the page, select Save.
The selected enumerated set is assigned to the tag.