Important: You do not have the latest version of Historian! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the Historian product page. For more information on upgrades, contact your Proficy sales agent or e-mail Proficy Sales Support. For the most up-to-date documentation, go here.
Assigning a Trigger Tag to an Unsolicited Calculation Tag
About this task
To assign an unsolicited trigger to a calculation tag and set up a dependency list:
Procedure
Select the tagname to which you want to apply the trigger.
In the Collection tab, select Unsolicited from the Collection Type drop-down list and specify an interval.
Select the Calculation tab.
Click Add to add a trigger.
The Insert Function Wizard opens.
Type the tagname directly into the Trigger Tag field, or click Browse to view the available tagnames.
Note: The Calculation Collector must be running if you want to browse for tags.
If you browsed for a tagname, select a tagname.
The wizard automatically populates the Trigger Tag field and updates the Function Preview field, as shown in the following figure:
Click Insert.
The trigger is added to the Calculation Triggers window, as shown in the following figure:
The trigger list also automatically populates when using the Insert Function wizard to build a calculation formula for an event based tag.