Implementing Tag Level Security
About this task
Set tag level security in the Historian Administrator. You do not need to use the Historian Security Groups for this security setting. You can use a Windows pre-defined group (power users, for example) or create your own separate group specifically for this function. For more information on creating and adding groups, refer to Setting Up Historian Security Groups.
Users must have iH Security Admins rights to set individual tag level security, browse, or query tags in the Historian Administrator.
Note: Tag security is not enforced in the Trend Client when it comes to browsing the full list of tags. Security, however, is enforced when it comes to trending data for tags for which you have permission. For example, if you are logged into the Trend Client as a user that is a member of the User Group assigned to a tag's security Read Group, you will still be able to browse all Historian tags. However, you are only allowed to trend the tags for which the user is a member of the User Group assigned to the tag's security Read Group,