Deleting A Tag

Procedure

  1. In the Tag Maintenance page, select a tag from the list in the left-hand window of the page.
    The tag information for that tag fills in the right-hand column.
  2. Select the Delete button at the bottom right of the page.
    The Delete Tag window shown in the following figure appears.

  3. Select the Remove Tag from System option and select OK.
    This removes the tag from the Tag Data-base but retains any data for that tag in the archive.
    Note: Since the tag data is still available from the archive, you can still reference that tag, for example, from within a calculation formula, or by using the Excel Add-In.
    A message box appears asking you to confirm the deletion.
  4. Select Yes to delete the tag.