To select a driver:
- In the spreadsheet, select the tags you want to add to your database.
- On the iFIX Wizards
toolbar, click the
Driver Wizard button. The Select Driver page of the Select Driver Wizard appears.
- From the list of available drivers, select the driver you want.
NOTES:
- The available driver(s) depends on the Discovery Agent you are using.
- If the appropriate driver is not installed on the target application, an error message is displayed. For information about this error message, refer to Troubleshooting the Driver Wizard.