To define the
default startup profile:
- In Classic view, in the iFIX WorkSpace, on the toolbar, click the Startup Profile Manager button.
-Or-
In Ribbon view, on the Applications tab, in the Utilities group, click Utilities, and then click Startup Profile Manager.
NOTE: The Startup Profile Manager can also be accessed from the Start menu by pointing to Programs, iFIX, Tools, and then Startup Profile Manager.
- On the Settings menu, click Default Startup Profile.
- In the Default Client SCU area, select the Enable Default SCU check box and enter an SCU file name.
- In the Default iFIX Startup Options area, select the check boxes that you want to apply to all iFIX users without a startup profile.
- If you plan to run iFIX as a service, in the Default Service SCU area, enter or select the Default Service Startup Parameter, and enter the node name and SCU file name of the service. This enables you configure the startup profile that iFIX uses when it runs as a service.
- Click OK.
NOTE: If you select the Enable the Default SCU option, make sure you also enable the global security paths (Use These Paths for All Startup Profiles) option in the Configuration dialog box in the Security Configuration application.