To edit a startup
profile:
- In Classic view, in the iFIX WorkSpace, on the toolbar, click the Startup Profile Manager button.
-Or-
In Ribbon view, on the Applications tab, in the Utilities group, click Utilities, and then click Startup Profile Manager.
NOTE: The Startup Profile Manager can also be accessed from the Start menu by pointing to Programs, iFIX, Tools, and then Startup Profile Manager.
- Select the profile that you want to edit.
- Double-click the row for that startup profile, or click the Edit button.
- Make the applicable changes to any of the following fields:
- iFIX Nodename field – the name of the iFIX node that you want to associate with this user.
- SCU File field – the location and name of the iFIX SCU file that you want to associate with this user.
- Allow User to Run Sample System check box – if selected, the specified Windows user can start the sample system from the iFIX Startup dialog box. The Sample System in no longer supported in iFIX 5.8 and greater.
- Allow User to Modify Nodename and SCU check box – if selected, the specified Windows user can edit these fields from the iFIX Startup dialog box.
NOTE: If you clear both the Allow User to Run Sample System and the Allow User to Modify Nodename and SCU check boxes, the iFIX Startup dialog box does not appear for the specified user.
- Click OK.
See Also