The Database Dynamo Configuration Utility (BTKCFG) supports the following command-line parameters:
NOTE: If you do not specify a slot number with the /N command line, you will get the next available slot. ExampleAn example that uses both command line parameters is as follows: BTKCFG /ABTK_AIS /N122 NOTE: If the block has already been configured, it should NOT be configured again.
|
Important Notice You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the iFIX product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com. For the most up-to-date documentation, go here. |
![]() |