Editing the Export File

Once you export the database, you can edit it with any text editor. As you edit the export file, use the following guidelines:

  • Verify that each block name is 256 characters or less.
  • Ensure each block field is spelled correctly.
  • Confirm the block type matches one of the types listed in the Block Type Abbreviations table.

You can also enter comments into the export file by typing an exclamation point (!) as the first character on a line.

CSV File Format

For more intricate editing of the export file, you need to understand the file format. For example, an export file saved in CSV format lists each row of the spreadsheet as one row in the CSV file. Each block's fields appear delimited by commas. The first two fields of each block are:

A_NAME, A_TAG

You only need to enter values for these two fields when creating new blocks. If no additional field values are present, Database Manager creates the block using the default block values. However, by adding these optional values to a block entry, you can complete specific dialog box fields when the block is imported. For example, the following line creates an Analog Input block with a scan time of 1 minute:

 

AI, AI2, , , , 1M

GDB File Format

The format of the GDB file is different. It uses the syntax:

label :: field_value ; fieldname

The first two lines of each block entry are required and contain the block type and block name. Without these lines, Database Manager will not add the block to the database when you subsequently import it.

Subsequent lines in a block entry appear for each field on the block's configuration dialog box. Including these additional lines is optional. If no additional lines are present, Database Manager creates the block using the default block values. However, by adding these optional lines to a block entry, you can complete specific dialog box fields when the block is imported. For example, to set the scan time of the block AI1 to 5 seconds, the export file should contain the following information:

Block Type:: AI ;A_NAME

Tag Name :: AI1 ;A_TAG

 

Scan Time :: 5 ; A_SCANT

Block Type Abbreviations 

Block Type

Abbreviation

Analog Alarm

AA

Analog Input

AI

Analog Output

AO

Analog Register

AR

Boolean

BL

Calculation

CA

Dead Time

DT

Device Control

DC

Digital Alarm

DA

Digital Input

DI

Digital Output

DO

Digital Register

DR

Event Action

EV

Extended Trend

ETR

Fanout

FN

Histogram

HS

Lead Lag

LL

Multistate Digital Input

MDI

On-Off Control

BB

Pareto

PA

PID

PID

Program

PG

Ramp

RM

Ratio/Bias

RB

Signal Select

SS

SQL Data

SQD

SQL Trigger

SQT

Statistical Control

SC

Statistical Data

SD

Text

TX

Timer

TM

Totalizer

TT

Trend

TR

 

See Also

How Do I...

Important Notice

You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security.

For information on all the latest features, see the iFIX product page.

For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com.

For the most up-to-date documentation, go here.