Reloading Databases

Even though you can create multiple databases for a SCADA server, Database Manager can load and display only one of them at a time. You can load any database residing on the current SCADA server by selecting Reload from the Database menu. Reloading a database lets you:

  • Switch from one database to another.
  • Restore the database to its saved configuration.
  • Load a database after completing and saving modifications.
  • Place on scan the chains configured to begin processing when SAC starts.

Using the SCU, you can select the default database to load on start-up. When you load another database, it remains in memory until you restart iFIX. Refer to the Setting up the Environment manual for more information about specifying the database to load on start-up.

 

See Also

How Do I...

Important Notice

You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security.

For information on all the latest features, see the iFIX product page.

For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com.

For the most up-to-date documentation, go here.