Blocks placed in Automatic mode enter PAUT mode. The block remains in this state until SAC scans the block again. While in PAUT mode, SAC scans the block as if it were in Automatic mode. Example: Blocks in PAUT ModeFor blocks with short scan times, this means that the next scan time occurs relative to the last scan. For example, suppose SAC scans AI1 at 1:15:30. This block has a 30-second scan time. If an operator changes the block's mode to Automatic, SAC:
For blocks with long scan times, SAC synchronizes the next scan to the system clock. For example, assume AI2 has a one hour scan time and a 30-minute phase. If an operator places the block into Automatic mode, SAC:
See Also |
Important Notice You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the iFIX product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com. For the most up-to-date documentation, go here. |
![]() |