PurposeAdds the current value of one block to the TARGET value of another block. You can also use this command to set the target for any of the three stages of the Ramp block. SyntaxADDTAR block TO block NOTE: When specifying a Ramp block, ADDTAR adds the value to the first target value of the block, ADDTAR2 adds the value to the second target value, and ADDTAR3 adds the value to the third target value. If a target value that is outside the Ramp block's EGU range, the Ramp block clamps the value to its low and high EGU limits. AO blocks to not have target values. When using blocks like AO or AI, which do not have target values, use ADDOUT command. ExampleTo add the current value of the block AI3 to the block PID5, enter: ADDTAR AI3 TO PID5 To add the current value of the block AI10 to the second target value of RAMP6, enter: ADDTAR2 AI10 TO RAMP6
|
Important Notice You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the iFIX product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com. For the most up-to-date documentation, go here. |
![]() |