Calculation Block – Equations

In order for the Calculation block to compute its output correctly, you must enter an equation. In general, the equation syntax is:  

input operator input

where input is one of the block's inputs and operator is a mathematical symbol. You specify inputs in the equation by their letter. For example, if you enter DI1 into the Calculation block's B Input field, you would refer to it in the equation as B.

You can enter any operator listed in the following table:

Operator

Function

ABS(input)

Absolute value

SQRT(input)

Square root

EXP(input)

Anti-log

LOG(input)

Natural log

LOG10(input)

Base-10 log

INT(input)

Changes floating point values to integers

-

Unary minus (example, -A).

^

Raise to power, exponential.

*

Multiply

/

Divide

+

Add

-

Subtract (example, A-B)

<

Less than

>

Greater than

NOTE: When doing greater than or less than comparisons, the Calculation block passes a value of 1 to the next block if the statement is true. If the statement is false, the block passes a value of 0.

 

Important Notice

You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security.

For information on all the latest features, see the iFIX product page.

For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com.

For the most up-to-date documentation, go here.