PurposeCloses a digital block (sets the value equal to 1). The block reflects the new value based on its own scan period. You can also close SIM registers. SIM registers range from 0 to 2000. Bit values range from 0 to 15. SyntaxCLOSE block CLOSE register:bit ExampleTo close the Digital Output block DO1, enter: CLOSE DO1 To close SIM register 28:4, enter: CLOSE 28:4 NOTE: When using the CLOSE command to set a Digital Input block, the block must be in Manual mode. If you attempt to set a Digital Input block that is in Automatic mode with a CLOSE command, iFIX generates an error message and takes the Program block off scan.
|
Important Notice You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the iFIX product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com. For the most up-to-date documentation, go here. |
![]() |