Database and SAC System Fields

The following table lists the system fields for the iFIX database and the Scan, Alarm, and Control (SAC) program, and what each field displays.

The field...

Parameter...

Displays...

A_BLKS

Total number of tags processed

The number of blocks that SAC processed since iFIX started.

A_BPS

Number of tags processed per second

The number of blocks that SAC processed in the last second.

A_CPM

SAC cycles per minute

The number of scans that SAC completes per minute with no overruns. SAC attempts to complete 60 scans per minute or 1200 scans if you are using subsecond processing. If the number in this field is less than 60 or 1200, your SCADA server is overloaded.

A_CPS

SAC cycles per second

The number of scans SAC completes per second with no overruns. SAC attempts to complete 1 scan per second or 20 scans if you are using subsecond processing. If the number in this field is less than 1 or 20, your SCADA server is overloaded.

A_DBNAM

Database name

The name of the database on the local SCADA server.

A_NDATE

Node date

The current date of the local SCADA server.

A_NODE

Node name

The name of the local SCADA server.

A_NTIME

Node time

The time of the local SCADA server.

A_PDBSN

Database serial number

The serial number of the process database.

A_SACOU

SAC output status

Enable, if SAC writes operator entries to the process hardware, or
Disable if SAC writes operator entries to the process database and not to the process hardware.

A_SACOV

Number of SAC overruns

The number of times that the Scan, Alarm, and Control (SAC) program could not execute all requests during a scan. The count begins from the time the SCADA server started.

A_SACPR

Alarm priority level

The SCADA server's alarm priority: INFO, LOLO, LOW, MEDIUM, HIGH, HIHI, or CRITICAL.

A_SACST

SAC scan status

RUN if SAC is scanning the process database, or STOP if SAC is not running.

 

Important Notice

You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security.

For information on all the latest features, see the iFIX product page.

For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com.

For the most up-to-date documentation, go here.