The field...
|
Displays...
|
Valid Entry
|
A_AACK
|
A block and field name pair to use for alarm acknowledgment.
|
Block.field
|
A_ADI
|
The block's alarm areas.
|
N/A. This field is provided for backward compatibility.
|
A_ALMCK
|
The block's alarm condition.
|
None, Close, Open, or Change of State.
|
A_ALMEXT1 A_ALMEXT2
|
The text entered in the block's alarm extension fields.
|
Up to 79 characters.
|
A_ALMINTIME
|
The time and date at which the block generated the
alarm.
|
N/A. This is a display only field.
|
A_ALMLASTTIME
|
The time and date at which the block last generated
an alarm.
|
N/A. This is a display only field.
|
A_ALMOCCUR F_ALMOCCUR
|
The number of times a block goes in and out of alarm
before it is acknowledged.
|
N/A. This is a display only field.
|
A_ALMSHELFREMTIME
F_ALMSHELFREMTIME
|
The remaining time left for a shelved alarm. |
N/A. This is a display only field. |
A_ALMSHELVED
F_ALMSHELVED
|
Indicates whether a specified alarm is shelved (YES/NO). |
N/A. This is a display only field. |
A_ALMSHELVEPOLICY
|
The name of alarm shelving policy. |
N/A. This is a display only field. |
A_ALMSHLVENAB
F_ALMSHLVENAB
|
Defines whether alarm shelving is enabled (YES/NO) for a block. |
N/A. This is a display only field. |
A_IALMSHLVENAB
F_IALMSHLVENAB
|
The initial alarm shelving status (ENABLE/DISABLE) for a block. |
N/A. This is a display only field. |
A_ALMSN
|
The serial number of the alarm area database.
|
N/A. This is a display only field.
|
A_ALM_SUSPENDMODE
F_ALM_SUSPENDMODE
|
Configures Event messaging (Suspend mode), which applies to the process alarm limit as an event. |
Enable: Yes (1), or Disable: No (0).
|
A_AREA1 through A_AREA15
|
The alarm areas assigned to the block.
|
ALL or an alarm area name.
|
A_ASUSP
|
A block and field that controls whether the Digital
Alarm block processes alarms.
NOTE: If
you use this field, you subsequently cannot use the A_ENAB or F_ENAB field
to disable or enable an alarm status. The A_ASUSP field takes precedence
over the A_ENAB or F_ENAB fields.
|
Block.field
|
A_AUTO F_AUTO
|
The current automatic/manual status of the block.
|
Automatic (1) or Manual (0).
|
A_CCALM
|
The digital block to close when an alarm occurs.
|
FIX32.node.block.field.
|
A_CCMOD
|
When to open the block's contact
|
Acknowledge, Return, All Clear, or Never.
|
A_CHALM
|
The chain's most severe alarm.
|
N/A. This is a display only field.
|
A_CLOSE
|
The first seven characters of the block's close label.
|
N/A. This field is provided for backward compatibility.
|
A_CLOSEDESC
|
Text in the block's Close field.
|
Up to 16 characters.
|
A_COMM_SURPRESS F_COMM_SURPRESS
|
Sets whether COMM alarms are suppressed for this block.
When selected, this option separates the original
alarm condition from the COMM alarm, and returns the block to the same
state as it was prior to a COMM alarm. For example, if prior to the COMM
alarm, the AA block was an active alarm but already acknowledged, that
is the state it should return to after communication is restored.
If disabled, AA blocks handle one alarm at a time.
As a result, it is possible that acknowledgement of a COMM alarm could
cause the ACK bit in the PLC to be written, and the original alarm condition,
if already acknowledged, could re-alarm.
|
Enable (1) or Disable (0).
|
A_CTK_PERSIST F_CTK_PERSIST
|
Sets whether blocks allow write attempts to the contact(s)
with every scan, even if the value being written is unchanged.
When disabled, the AA block only attempts to write
to the defined contact tag when a value has changed and it needs to be
written to the PLC. The write is a one-time attempt, so if it fails, the
write will not be retried until the block needs to write a new value.
NOTE: There
are four modes for the contacts - “Acknowledge”, “Return”, “All Clear”,
and “Never” - that control when the contact is cleared. Since the contact
mode of “Never” does not reset the contact, the Continuous Output option
is not supported for this contact mode.
|
Enable (1) or Disable (0).
|
A_CUALM
|
The block's current alarm.
|
N/A. This is a display only field.
|
A_CV F_CV
|
The block's current value.
|
A numeric value within the EGU range.
|
A_DALM F_DALM
|
Whether to delete alarm from summary queue after acknowledgment.
|
0 (false) or 1 (true).
|
A_DELAY
|
The length of time to wait before generating an alarm.
|
Any time from 00:00:00:00 to 03:00:00:00 (up to 3
days, in the time format of dd:hh:mm:ss).
|
A_DESC
|
The text in the block's Description field.
|
Up to 256 characters.
|
A_ENAB F_ENAB
|
The block's alarm status.
NOTE: The
A_ASUSP field takes precedence over the A_ENAB or F_ENAB fields. In other
words, after you use the A_ASUSP field, you cannot use the A_ENAB or F_ENAB
field to disable or enable an alarm status.
|
Enable: Yes (1), or Disable: No (0).
|
A_EOUT
|
Yes, if the block writes data to the process hardware
or No, if the block does not.
|
Yes or No.
|
A_ESIGACK F_ESIGACK
|
Whether operators are allowed to acknowledge alarms
for this tag without entering a signature, even if this tag requires electronic
signatures for data entry.
|
Yes or No.
|
A_ESIGCONT F_ESIGCONT
|
If allow continuous use is enabled for this tag.
|
Yes or No.
|
A_ESIGREQ_COMMENT
F_ESIGREQ_COMMENT
|
A comment is required when using an electronic signature. |
Enable: Yes (1), or Disable: No (0).
|
A_ESIGTRAP F_ESIGTRAP
|
Whether unsigned writes are accepted or rejected by
this tag or accepted and logged.
|
ACCEPT, LOG, REJECT.
|
A_ESIGTYPE F_ESIGTYPE
|
The signing requirements for this tag.
|
None, PERFONLY, or PERFVERI.
|
A_EVENT
|
The initial event messaging status.
|
N/A. This is a display only field.
|
A_HIST_COLLECT F_HIST_COLLECT
|
Sets whether or not this block is under collection.
|
Yes (1) or No (0).
|
A_HIST_COMPRESS F_HIST_COMPRESS
|
Sets whether or not compression is used by the Collector.
|
Enable (1) or Disable (0).
|
A_HIST_COMPTIME F_HIST_COMPTIME
|
The Collector compression time out.
|
A positive numeric value (0 or greater), in milliseconds.
|
A_HIST_COMPTYPE F_HIST_COMPTYPE
|
The type of Collector deadband setting.
|
Absolute (0) or Percentage (1).
|
A_HIST_DEADBAND F_HIST_DEADBAND
|
The Collector deadband setting.
|
A positive numeric value (0 or greater).
|
A_HIST_DESC
|
The GE Historian description.
|
String; maximum of 128 characters.
|
A_HIST_INTERVAL F_HIST_INTERVAL
|
The collection interval for this block. The value
of this field must be greater than the value of the A_HIST_OFFSET and
F_HIST_OFFSET fields.
Use the following formula to determine if the entered
value is acceptable for this field.
A_/F_HIST_INTERVAL > A_/F_HIST_OFFSET * 1000
NOTE: The values for the A_HIST_OFFSET and F_HIST_OFFSET
fields are in seconds.
|
A float value, in milliseconds. Values must be entered
in increments of 100. Minimum value: 100 ms.
|
A_HIST_OFFSET F_HIST_OFFSET
|
The collection offset time. The value of this field
must be less than or equal to the value of the A_HIST_INTERVAL and F_HIST_INTERVAL
fields.
Use the following formula to determine if the entered
value is acceptable for this field.
A_/F_HIST_OFFSET ≤ A_/F_HIST_INTERVAL / 1000
NOTE: The values for the A_HIST_INTERVAL and F_HIST_INTERVAL
fields are in milliseconds.
|
A numeric value, in seconds. Must use whole numbers.
|
A_HIST_TIMERES F_HIST_TIMERES
|
The collection time resolution.
|
Milliseconds(0) or Seconds (1).
|
A_IAM
|
The initial Automatic/Manual status of the block.
|
Automatic or Manual.
|
A_IENAB
|
The initial alarm status.
|
N/A. This is a display only field.
|
A_INV
|
Yes, if the block inverts its output value or No, if the block does not invert its output value.
|
Yes or No.
|
A_IOAD
|
The block's I/O address.
|
Depends on your driver. Refer to your driver manual
for more information.
|
A_IODV
|
The name of the block's I/O driver.
|
Depends on your driver. Refer to your driver manual
for more information.
|
A_IOHT
|
The I/O driver's hardware options.
|
Depends on your driver. Refer to your driver manual
for more information.
|
A_ISCAN
|
The initial scan status (on or off) of the block.
|
On or Off.
|
A_LAALM
|
The block's most severe unacknowledged alarm. If no
unacknowledged alarm exists, the current alarm is displayed.
|
N/A. This is a display only field.
|
A_NALM F_NALM
|
Yes or 1, if the block has unacknowledged alarms or
No or 0, if the block has no unacknowledged alarms.
|
N/A. This is a display only field.
|
A_NAME
|
The block's type, for example AI for an Analog Input
block.
|
N/A. This is a display only field.
|
A_NAREA
|
Enters a new alarm area in the alarm area database.
|
N/A. This is a write only field.
|
A_NEXT
|
The name of the next block in the chain.
|
N/A. This is a display only field.
|
A_OPCLIMIT
|
The hardware options of the OPC server.
|
N/A. This is a display only field.
|
A_OPCQLTY
|
The quality status of the OPC server.
|
N/A. This is a display only field.
|
A_OPCSUBSTAT
|
The quality substatus of the OPC server.
|
N/A. This is a display only field.
|
A_OPCTIME
|
The time and date from the OPC server.
|
N/A. This is a display only field.
|
A_OPEN
|
The first seven characters of the block's open label.
|
N/A. This field is provided for backward compatibility.
|
A_OPENDESC
|
Text in the block's Open field.
|
Up to 16 characters.
|
A_PDR_ACCESSTIME F_PDR_ACCESSTIME
|
Reserved. |
N/A. |
A_PDR_ARRAYLENGTH F_PDR_ARRAYLENGTH
|
Reserved. |
N/A. |
A_PDR_DEADBAND F_PDR_DEADBAND
|
Reserved. |
N/A. |
A_PDR_DISABLEOUT F_PDR_DISABLEOUT
|
Reserved. |
N/A. |
A_PDR_LATCHDATA F_PDR_LATCHDATA
|
Reserved. |
N/A. |
A_PDR_UPDATERATE F_PDR_UPDATERATE
|
Reserved. |
N/A. |
A_PREV
|
The name of the previous block in the chain.
|
N/A. This is a display only field.
|
A_PRI
|
The block's alarm priority.
|
Low, Medium, or High.
|
A_PRIM
|
The block's name.
|
N/A. This is a display only field.
|
A_REALM
|
The length of time to wait before re-issuing an alarm.
|
Any time from 00:00:00:00 to 03:00:00:00 (up to 3
days, in the time format of dd:hh:mm:ss).
|
A_SA1 through A_SA3
|
The security areas assigned to the block.
|
Up to three security area names.
|
A_SCAN
|
The on/off scan status of the block.
|
On or Off.
|
A_SCANT
|
The block's scan time and phase.
|
E for exception-based processing, 0 for one shot processing,
or time:phase for time-based processing.
|
A_TAG
|
The block's name.
|
N/A. This is a display only field.
|
A_WARM
|
Yes or No.
|
N/A. This is a display only field.
|
A_ALMACK F_ALMACK
|
Reserved. |
N/A. |
A_ALMCHANGE F_ALMCHANGE
|
Reserved. |
N/A. |
A_ALMDELETE F_ALMDELETE
|
Reserved. |
N/A. |
A_ALMGEN F_ALMGEN
|
Reserved. |
N/A. |
A_ALMRESET F_ALMRESET
|
Reserved. |
N/A. |
A_ALMUPDATE F_ALMUPDATE
|
Reserved. |
N/A. |
A_PUBLISH F_PUBLISH
|
Reserved. |
N/A. |
A_WRITABLE F_WRITABLE
|
Reserved. |
N/A. |