The Event Action block tests the value or alarm condition of the previous block using IF-THEN-ELSE logic. In the IF portion of the logic, you can specify the value or alarm condition for which you want to test.
If the condition is true, the block's THEN logic executes. If the condition is false, the block's ELSE logic. Valid operators and conditions include:
|
Important Notice You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the iFIX product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com. For the most up-to-date documentation, go here. |
![]() |