To import a database:
IMPORTANT:
Be aware that before you perform a large import, you should adjust the
spreadsheet refresh rate to 20 or more seconds. If you leave the refresh
rate at a low number, such as the default of 5 seconds, and you try to
import a large amount of tags, the database may appear unresponsive. To
adjust the refresh rate, in Classic view, on the Tools menu, click Options,
or in Ribbon view, on the Home tab, in the Settings group, click Options,
and then edit the value for the Spreadsheet Auto Refresh field, if it's
enabled. After this is done, you can import the database.
- In the Database Manager,
in Ribbon view, on the Home tab, in the Process Database group, click
Import.
- Or -
In Classic view, on the Database Menu, click
Import.
The following
text appears:
SAC will be stopped while blocks are being imported and then restarted.
- Select OK
to acknowledge the message.
- Select the file you
want to import.
NOTES:
- If you are
using GE Historian as your Historian and you import and open a database
on a machine that does not have GE Historian 3.1 or above installed,
fields added for Historian collection are disabled. Additionally, the
values for Historian fields are retained.
- If you enabled
Automatically Configure Tags for Collection in Historian on the
Historian tab of the User Preferences dialog box, then:
- All
imported tags will be added to the default collector and collection by
GE Historian are enabled.
- If you
have an existing database and import a new database and both databases
contain a tag with the same name, the existing database tag are overwritten
by the new database tag.
- If you
have an existing database and those tags are not enabled for collection
in Historian, at reload time the tags are not enabled for collection.
In other words, this setting does not override Historian's settings.