The field...
|
Displays...
|
Valid Entry
|
A_ADI
|
The block's alarm areas.
|
N/A. This field is provided for backward compatibility.
|
A_ALMEXT1 A_ALMEXT2
|
The text entered in the block's alarm extension fields.
|
Up to 79 characters.
|
A_ALMINTIME
|
The time and date at which the block generated the
alarm.
|
N/A. This is a display only field.
|
A_ALMLASTTIME
|
The time and date at which the block last generated
an alarm.
|
N/A. This is a display only field.
|
A_ALMOCCUR F_ALMOCCUR
|
The number of times a block goes in and out of alarm
before it is acknowledged.
|
N/A. This is a display only field.
|
A_ALMSN
|
The serial number of the alarm area database.
|
N/A. This is a display only field.
|
A_AREA1 through A_AREA15
|
The alarm areas assigned to the block.
|
ALL or an alarm area name.
|
A_AUTO F_AUTO
|
The current automatic/manual status of the block.
|
Automatic (1) or Manual (0).
|
A_CHALM
|
The chain's most severe alarm.
|
N/A. This is a display only field.
|
A_CUALM
|
The block's current alarm.
|
N/A. This is a display only field.
|
A_CV E_CV F_CV
|
The block's current value.
|
A numeric value within the EGU range.
|
A_DALM F_DALM
|
Whether to delete alarm from summary queue after acknowledgment.
|
0 (false) or 1 (true).
|
A_DESC
|
The text in the block's Description field.
|
Up to 256 characters.
|
A_EGUDESC
|
The block's engineering units label.
|
Up to 33 characters.
|
A_EHI F_EHI
|
The block's high EGU limit.
|
A numeric value. The range between the low and high
values value cannot exceed 3.40282300000000e+38.
|
A_ELO F_ELO
|
The block's low EGU limit.
|
A numeric value. The range between the low and high
values value cannot exceed 3.40282300000000e+38.
|
A_ENAB F_ENAB
|
The block's alarm status.
|
Enable: Yes (1), or Disable: No (0).
|
A_ESIGACK F_ESIGACK
|
Whether operators are allowed to acknowledge alarms
for this tag without entering a signature, even if this tag requires electronic
signatures for data entry.
|
Yes or No.
|
A_ESIGCONT F_ESIGCONT
|
If allow continuous use is enabled for this tag.
|
Yes or No.
|
A_ESIGREQ_COMMENT
F_ESIGREQ_COMMENT
|
A comment is required when using an electronic signature. |
Enable: Yes (1), or Disable: No (0).
|
A_ESIGTRAP F_ESIGTRAP
|
Whether unsigned writes are accepted or rejected by
this tag or accepted and logged.
|
ACCEPT, LOG, REJECT.
|
A_ESIGTYPE F_ESIGTYPE
|
The signing requirements for this tag.
|
None, PERFONLY, or PERFVERI.
|
A_ETAG
|
The first four characters of the block's engineering
units label.
|
N/A. This field is provided for backward compatibility.
|
A_EVENT
|
The initial event messaging status.
|
N/A. This is a display only field.
|
A_HIST_COLLECT F_HIST_COLLECT
|
Sets whether or not this block is under collection.
|
Yes (1) or No (0).
|
A_HIST_COMPRESS F_HIST_COMPRESS
|
Sets whether or not compression is used by the Collector.
|
Enable (1) or Disable (0).
|
A_HIST_COMPTIME F_HIST_COMPTIME
|
The Collector compression time out.
|
A positive numeric value (0 or greater), in milliseconds.
|
A_HIST_COMPTYPE F_HIST_COMPTYPE
|
The type of Collector deadband setting.
|
Absolute (0) or Percentage (1).
|
A_HIST_DEADBAND F_HIST_DEADBAND
|
The Collector deadband setting.
|
A positive numeric value (0 or greater).
|
A_HIST_DESC
|
The GE Historian description.
|
String; maximum of 128 characters.
|
A_HIST_INTERVAL F_HIST_INTERVAL
|
The collection interval for this block. The value
of this field must be greater than the value of the A_HIST_OFFSET and
F_HIST_OFFSET fields.
Use the following formula to determine if the entered
value is acceptable for this field.
A_/F_HIST_INTERVAL > A_/F_HIST_OFFSET * 1000
NOTE: The values for the A_HIST_OFFSET and F_HIST_OFFSET
fields are in seconds.
|
A float value, in milliseconds. Values must be entered
in increments of 100. Minimum value: 100 ms.
|
A_HIST_OFFSET F_HIST_OFFSET
|
The collection offset time. The value of this field
must be less than or equal to the value of the A_HIST_INTERVAL and F_HIST_INTERVAL
fields.
Use the following formula to determine if the entered
value is acceptable for this field.
A_/F_HIST_OFFSET ≤ A_/F_HIST_INTERVAL / 1000
NOTE: The values for the A_HIST_INTERVAL and F_HIST_INTERVAL
fields are in milliseconds.
|
A numeric value, in seconds. Must use whole numbers.
|
A_HIST_TIMERES F_HIST_TIMERES
|
The collection time resolution.
|
Milliseconds (0) or Seconds (1).
|
A_IAM
|
The initial Automatic/Manual status of the block.
|
Automatic or Manual.
|
A_IENAB
|
The initial alarm status.
|
N/A. This is a display only field.
|
A_ISCAN
|
The initial scan status (on or off) of the block.
|
On or Off.
|
A_K
|
The scaling factor used to modify the lead lag curve.
|
-100.00 to 100.00
|
A_LAALM
|
The block's most severe unacknowledged alarm. If no
unacknowledged alarm exists, the current alarm is displayed.
|
N/A. This is a display only field.
|
A_LAG
|
The block's lag time constant.
|
0 to 100.00.
|
A_LEAD
|
The block's lead time constant.
|
0 to 100.00.
|
A_NALM F_NALM
|
Yes or 1, if the block has unacknowledged alarms or
No or 0, if the block has no unacknowledged alarms.
|
N/A. This is a display only field.
|
A_NAME
|
The block's type, for example AI for an Analog Input
block.
|
N/A. This is a display only field.
|
A_NAREA
|
Enters a new alarm area in the alarm area database.
|
N/A. This is a write only field.
|
A_NEXT
|
The name of the next block in the chain.
|
N/A. This is a display only field.
|
A_OPCLIMIT
|
The hardware options of the OPC server.
|
N/A. This is a display only field.
|
A_OPCQLTY
|
The quality status of the OPC server.
|
N/A. This is a display only field.
|
A_OPCSUBSTAT
|
The quality substatus of the OPC server.
|
N/A. This is a display only field.
|
A_OPCTIME
|
The time and date from the OPC server.
|
N/A. This is a display only field.
|
A_PDR_ACCESSTIME F_PDR_ACCESSTIME
|
Reserved for future use.
|
A_PDR_ARRAYLENGTH F_PDR_ARRAYLENGTH
|
Reserved for future use.
|
A_PDR_DEADBAND F_PDR_DEADBAND
|
Reserved for future use.
|
A_PDR_DISABLEOUT F_PDR_DISABLEOUT
|
Reserved for future use.
|
A_PDR_LATCHDATA F_PDR_LATCHDATA
|
Reserved for future use.
|
A_PDR_UPDATERATE F_PDR_UPDATERATE
|
Reserved for future use.
|
A_PREV
|
The name of the previous block in the chain.
|
N/A. This is a display only field.
|
A_PRI
|
The block's alarm priority.
|
Low, Medium, or High.
|
A_PRIM
|
The block's name.
|
N/A. This is a display only field.
|
A_SA1 through A_SA3
|
The security areas assigned to the block.
|
Up to three security area names.
|
A_SCAN
|
The on/off scan status of the block.
|
On or Off.
|
A_SCANT
|
The block's scan time and phase.
|
E for exception-based processing, 0 for one shot processing,
or time:phase for time-based processing.
|
A_TAG
|
The block's name.
|
N/A. This is a display only field.
|
A_WARM
|
Yes or No.
|
N/A. This is a display only field.
|
A_ALMACK F_ALMACK
|
Reserved for future use.
|
A_ALMCHANGE F_ALMCHANGE
|
Reserved for future use.
|
A_ALMDELETE F_ALMDELETE
|
Reserved for future use.
|
A_ALMGEN F_ALMGEN
|
Reserved for future use.
|
A_ALMRESET F_ALMRESET
|
Reserved for future use.
|
A_ALMUPDATE F_ALMUPDATE
|
Reserved for future use.
|
A_PUBLISH F_PUBLISH
|
Reserved for future use.
|
A_WRITABLE F_WRITABLE
|
Reserved for future use.
|