PurposeDefines the time the block waits for the condition specified in a subsequent WAITFOR or WAITSTAT command to occur. SyntaxMAXWAIT value Parametervalue – specifies the number of seconds (0-32767 seconds) you want to wait. The value you enter should be an exact multiple of the chain's scan time. If it is not, the value is rounded to the next highest multiple of the block's scan time at run-time. Note that the value 0 means to wait forever. For example, if you specify a MAXWAIT of 60 seconds and the block has a scan block of 25 seconds, the MAXWAIT command suspends the block for 75 seconds because the MAXWAIT period extended into the block's third scan period.ExamplesThe MAXWAIT command applies to all subsequent WAITSTAT and WAITFOR commands unless another MAXWAIT command occurs. For example: MAXWAIT 60 In this program, the block waits a maximum of 60 seconds for PID1 to be switched to Automatic mode and another 60 seconds for the output of AI1 to equal 10. But the block only waits a maximum of 5 seconds for SUBPROG1 to be placed on scan. The MAXWAIT command also applies to called Program blocks. For example: MAXWAIT 60 These commands instruct the Program block to wait a maximum of 60 seconds before it switches AI1 to Automatic mode. The SETAUTO command is then processed within 60 seconds regardless of whether PROG2 has processed all of its commands.
|
Important Notice You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the iFIX product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com. For the most up-to-date documentation, go here. |
![]() |