On-Off Control Block Example

The On-Off Control block uses contact inputs to implement on-off control based on an analog value. For example, as the following figure shows, the High Contact Data fields can open a valve to add hot water to a tank when the temperature reading falls below a specified value. In turn, the block can turn off the hot water when the temperature reaches a specified value.  

In addition, the Low Contact Data fields can trigger a cold water valve to close when the temperature falls below a specified value and to open when the reading rises above the value.

 

Important Notice

You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security.

For information on all the latest features, see the iFIX product page.

For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com.

For the most up-to-date documentation, go here.