OPEN Command

Purpose

Opens a digital block (sets the value equal to 0). The block reflects the new value based on its own scan period.

You can also open SIM registers. SIM registers range from 0 to 2000. Bit values range from 0 to 15.

Syntax

OPEN block

OPEN register:bit

NOTE: When using the OPEN command to set a Digital Input block, the Digital Input block must be in Manual mode before it can be set. If you attempt to set a Digital Input block that is in Automatic mode with an OPEN command, iFIX generates an error message and takes the Program block off scan.

 

Important Notice

You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security.

For information on all the latest features, see the iFIX product page.

For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com.

For the most up-to-date documentation, go here.