Ramp Block Example

The Ramp block can ensure the stability of a motor that is essential to a start up process. The block assists in the ramp and soak methods used to bring the motor up to full speed by directing the increase and hold time in RPMs during three defined stages:  

In the first stage, the block ramps up to the Target 1 value based upon the increments specified in the Ramp Rate 1 field. When the Target 1 value is reached, the block continues to output the Target 1 value for the period specified in the Hold Time 1 field. After this period has expired, the block repeats the process for ramp stages 2 and 3.

NOTE: If a Ramp rate is 0.00, the stage is not executed.

 

Important Notice

You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security.

For information on all the latest features, see the iFIX product page.

For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com.

For the most up-to-date documentation, go here.