PurposeRuns FIX or third-party applications. For example, you can use this command to automatically download a recipe or save the process database. This command can also launch third-party applications such as Windows Notepad. SyntaxRUNTASK executable [command line parameter] Parametersexecutable – specifies the name of the .EXE file for the application you want to run. This parameter can include path information, but not wildcards. For example: RUNTASK C:\PROGRAMS\MYPROG.EXE command line parameter – specifies any applicable command line parameters for the executable, enclosed in quotes. Up to 128 characters can be used to define command line parameters. Command line parameters are available for the following iFIX applications:
|
Important Notice You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the iFIX product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com. For the most up-to-date documentation, go here. |
|