SQL Trigger Blocks in Manual Mode

SQL Trigger blocks automatically execute SQL commands when placed in Automatic mode, not in Manual mode. However, an operator can manually trigger a SQL Trigger block through a Data link that uses the A_TRIP field or through the Database Manager. When manually triggered, the block executes SQL commands as if it were in Automatic mode.

If an SQL Trigger block is monitoring the CLOSE to OPEN state of a digital block, the SQL Trigger block activates when the digital block opens. If the SQL Trigger block is placed in Manual mode before the digital block opens, the SQL Trigger block does not activate until it is switched to Automatic mode.  

 

Important Notice

You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security.

For information on all the latest features, see the iFIX product page.

For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com.

For the most up-to-date documentation, go here.