Statistical Data Block – Formulas

In the following table, n represents the number of observations and g is the number of groups.

Formula

Abbreviation

Description

XBAR

The group average.

XBARBAR

The average of the group average.

R=Xmax - Xmin

R

The range of the group.

RBAR

The average range of all groups.

S

The standard deviation of the group.

SBAR

The average of sample standard deviations.

UCLX
LCLX

The upper and lower control limits*.

UWLX
LWLX

The upper and lower warning limits*.

UCLR
LCLR

The upper and lower control limit for range.

UCLs
LCLs

The upper and lower control limits for the standard deviation.

Sigma

The process standard deviation.


ZU


ZL

The upper and lower CPK limit.

CPK=MIN(ZU,ZL) / 3.0

CPK

The process capability index.

*NOTE: The block sets the upper (USLX) and lower (LSLX) user specification limits to values greater and less than the upper and lower control limits, respectively, if you do not specify a value.

A2 is the factor for control limits for X. D4 and D3 are factors for control limits for R. C4 is the divisor estimate of the standard deviation. Additional information on the control charts that these values are derived from can be found in the original text: ASTM publication STP-15D, Manual on the Presentation of Data and Control Chart Analysis, 1976; Pages 134-136.

 

See Also

Important Notice

You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security.

For information on all the latest features, see the iFIX product page.

For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com.

For the most up-to-date documentation, go here.