Alarms in the Boolean Block

To include an alarm as an input in a Boolean block calculation, you must use the following format:  

tag name:alarm type

Valid alarm types and their priorities include the following:

Priority

Alarm Type

Description

1

COMM

Communication Error (BAD value).

1

OCD

Open circuit detected.

1

IOF

General I/O Failure.

1

FLT

Floating Point Error.

1

OVER

Over Range.

1

UNDER

Under Range.

1

ERROR

Any Statistical Data block alarm.

2

CFN

Change from normal alarm (digital blocks only).

2

COS

Change of State alarm (digital blocks only).

2

HIHI

Block in HIHI alarm state.

2

LOLO

Block in LOLO alarm state.

3

RATE

Value exceeds rate-of-change setting.

3

HI

Block in HI alarm state.

3

LO

Block in LO alarm state.

4

DEV

Deviation Alarm.

5

OK

Block in normal state.

 

Important Notice

You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security.

For information on all the latest features, see the iFIX product page.

For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com.

For the most up-to-date documentation, go here.