Using Experts to Animate Objects

An easy way to animate objects is to use Experts. To access an Expert, click the button on the Experts toolbar that corresponds to the task you want to perform (Classic view), or on the Tool tab, in the Animations group, click Animations, and then choose the appropriate Expert (Ribbon view). Some Experts are only available using the Task Wizard. For example, if you want to animate the edge color of an oval, select the Edge Color Expert from the Animation category of the Task Wizard.

To learn more about the fields on the Expert, click the Help button on the Expert. For more information on iFIX Experts and the Task Wizard, refer to the Using Process Assistants to Expedite Pictures chapter.

Additionally, you can access some Experts from the Basic Animation dialog box. To open the Basic Animation dialog box, select Animations from the object's right-click menu.

See Also

Important Notice

You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security.

For information on all the latest features, see the iFIX product page.

For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com.

For the most up-to-date documentation, go here.