I/O drivers are started by the I/O Control program through the Task Configuration dialog box. When you install an I/O driver, the I/O Control program is automatically added to the list of tasks. If you remove the I/O Control program from the task list, you can add it back again. The table below shows you the command line parameters you can use to specify how I/O drivers start. NOTE: FIX I/O drivers 7.x or greater automatically start communicating with their OPC server. No command line parameter is needed.
See AlsoHow Do I... |
Important Notice You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the iFIX product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com. For the most up-to-date documentation, go here. |
![]() |