Memory Requirements

iClients and SCADA nodes (without Enhanced Failover or GE Historian) require at least 2 GB RAM. For better performance, please consider using more.

NOTE: As more applications run simultaneously on a SCADA server, performance decreases. Whenever possible, run additional applications on different computers.

If your picture cache size increases, your memory requirements should increase:

  • 2 to 3 times the file size for each picture that does not include bitmaps and controls.
  • 3 to 4 times the file size for each picture that includes bitmaps and controls.

For example, a 2 megabyte file that does not include bitmaps and controls requires a 4 to 6 megabyte increase in memory. A 2 megabyte file that includes bitmaps and controls requires an increase in the memory of 6 to 8 megabytes.

Important Notice

You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security.

For information on all the latest features, see the iFIX product page.

For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com.

For the most up-to-date documentation, go here.