iFIX supports the following regional settings available in the Windows Control Panel:
NOTE: The decimal symbol and the digit grouping symbol cannot be the same character. Also, the time separator and the date separator cannot be the same character. Formatting the Time and DateAvoid changing the time style or short date style in regional settings to values that are outside of the standard styles provided. Changing these values to non-standard styles may result in improperly formatting times and dates in some parts of iFIX. iFIX supports the following short date formats, some of which may not be available in certain language versions of Windows:
Formatting the Regional Language SettingAvoid changing the language setting once a timer has been used in a schedule. If changed, the date always reverts to 30/12/99, regardless of what you set the start time to be. Setting the System Default LocaleThe selected locale must be set as the system default. |
Important Notice You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the iFIX product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com. For the most up-to-date documentation, go here. |
![]() |