iFIX ODBC provides communication between relational databases and the iFIX database. The iFIX database can be configured to communicate based on an event, a time, or a combination of both. iFIX ODBC consists of the: The SQL task performs the following functions:
The SQL Trigger block defines:
The SQL Data block defines:
Both database blocks communicate with the SQL task, WSQLODC.EXE. This task runs on a SCADA node and handles communication with the ODBC driver. If the connection to the relational database is lost, SQL commands and data can be backed up. When the connection is re-established, SQL commands and data are executed in the order in which they were backed up. Refer to the Backing Up and Restoring Data section for a more detailed description of the back-up and restore process. NOTE: If you copy and paste the SQT and SQD blocks, they will not fire. You must create these blocks in full. See AlsoHow Do I... |
Important Notice You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the iFIX product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GEDigitalSalesSupport@ge.com. For the most up-to-date documentation, go here. |
![]() |