Setting Drawing Preferences

To set drawing preferences:

  1. In Classic view, from the iFIX WorkSpace menu, select User Preferences.

-Or-

In Ribbon view, on the Home tab, in the WorkSpace group, click Settings, and then click User Preferences.

  1. Click the Drawing Options tab.
  2. In the Extend Options area, select the default option for extending line objects to an intersection point.
  3. In the Trim Options area, select the default option for trimming line objects to an intersection point.
  4. Select the Always Show Connection Nodes check box to display the connection nodes when using the LineConnector Tool, the Rightangleline Connector, or the Pipe Connector.

 

See Also

Important Notice

You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security.

For information on all the latest features, see the iFIX product page.

For more information on upgrades, contact your GE Digital sales agent or e-mail GEDigitalSalesSupport@ge.com.

For the most up-to-date documentation, go here.