To set the OPC
connection error preferences:
- In Classic view,
from the iFIX WorkSpace menu, select User Preferences.
-Or-
In Ribbon view, on the Home tab, in the
WorkSpace group, click Settings, and then click User Preferences.
- Click the Animations
Data Error Defaults tab.
- In the Linear Animation
Object Defaults area, enter the default numeric values to use when an
error occurs scaling a value.
- In the Format Animations
Object Defaults area, enter the default strings to display in a Data link
when an error occurs.
- In the Numeric Table
Entries and the String Table Entries areas, enter the default numeric
and string values to use when an error occurs in a lookup table.
- In the Color Table
Entries area, click each button and select the color to use when an error
occurs in a lookup table.
See Also