Disabling Error Dialog Boxes

If an error occurs in the run-time environment, an error dialog box displays requiring user intervention. You can disable error dialog boxes for particular errors by editing the FILTEREDERRORS.INI file in the Local path. For example, you may want to suppress the error dialogs when network sessions are lost. In order to do this, add the error codes you want filtered in the INI file as follows:

;To add an error code to be filtered increment the count and set

;the Error equal to the return code

 

[ErrorCodes]

Count = 4

Error1 = 1620

Error2 = 1914

Error3 = 1915

Error4 = 8517

In this example, all typical network session errors are suppressed.

After you edit the FILTEREDERRORS.INI file, restart the WorkSpace to ensure your changes take effect.

See Also

Important Notice

You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security.

For information on all the latest features, see the iFIX product page.

For more information on upgrades, contact your GE Digital sales agent or e-mail GEDigitalSalesSupport@ge.com.

For the most up-to-date documentation, go here.