The Environment Protection tab of the User Preferences dialog box displays
the following items:
Enable Run Time Environment Protection
Select this check box to enable environment protection for the local
node. When
enabled, you can select the specific options that you want to restrict
access to. These options take effect when you switch to the run-time environment.
WorkSpace Title and Menu Options
Item
|
Description
|
Disable Title Bar And Menu Bar
|
Select this check box to hide the WorkSpace menu bar
and title bar at run-time.
NOTE: In
Ribbon view, if this option is selected, the Title Bar takes on the appearance
of Classic view, rather than Ribbon view.
|
Disable Menu Bar
|
Select this check box to hide the WorkSpace menu bar
and title bar at run-time.
|
Disable "WorkSpace" Menu Pulldown
|
Select this check box to disable the WorkSpace menu
at run-time.
|
NOTES:
- When
WorkSpace is running with the Ribbon in full screen mode and you enable
the Run
Time Environment Protection and Disable Title bar and Menu Bar options,
the Ribbon bar will be displayed when the Alt key is pressed. This will
allow access to the Historical tab with Global Time Control. All other
menus will be removed or disabled and the WorkSpace cannot be dragged,
minimized, or closed using the Ribbon bar.
- The
historical tab with Global Time Control can be removed by modifying the
DyanmicRibbon.ini file in the iFIX install ADDON folder and setting [StandardTabs]
Historical=0. If the tab is removed and no other tabs are visible on the
run mode Ribbon (because you also enabled the enable the Run
Time Environment Protection and Disable Title bar and Menu Bar options)
, the Ribbon bar will not display when the Alt key is pressed.
WorkSpace File Menu Accelerators
Item
|
Description
|
Disable "WorkSpace" File Menu Accelerators
|
Select this check box to disable both the Open (Ctrl+O)
and Print (Ctrl+P) WorkSpace file menu accelerators while in the Run-time
environment.
|
Disable Open Accelerator
|
Select this check box to disable the Open (Ctrl+O)
WorkSpace file menu accelerator while in the Run-time environment.
|
Disable Print Accelerator
|
Select this check box to disable the Print (Ctrl+P)
WorkSpace file menu accelerator while in the Run-time environment.
|
Other Options
Item
|
Description
|
Disable <Ctrl> <Alt> <Del>
|
Select this check box to disable the <Ctrl><Alt><Delete>
key sequence at run-time, thereby restricting operators from accessing
the Task Manager, changing their password, logging off, or shutting down
the computer.
|
Disable Task Switching
|
Select this check box to disable run-time task switching
through <Alt><Tab> and the Start button.
NOTE: The
Shift + F10 key macro does not work if you select this option.
|
Disable VBE Access
|
Select this check box to allow you to restrict access
to the Visual Basic Editor at run-time. If
access is not restricted, the editor appears when a compilation or run-time
error occurs, allowing you to correct the error. When
you restrict access, the iFIX WorkSpace suppresses the Visual Basic Editor
even if an error occurs.
|
How
Do I...