The OPC Client I/O driver allows you to bring OPC data into and out of iFIX. It is automatically installed with iFIX; however, if you choose to create a customized install program, the OPC Client I/O driver is an optional component.
To use the OPC I/O Driver:
- In the Database Manager, in the Driver field for the primary block, select OPC - OPC Client vx.xx from the list.
- Click the Browse button next to the I/O Address field. The Browse I/O Address dialog box appears.
- Select an I/O point from an available server and group, and then click OK to exit the dialog box. The I/O Address field will display the following:
Server;Group;ItemID[;AccessPath]
When you click out of the I/O Address field, ;No Access Path will be appended to the existing text, like this:
Server;Group;ItemID;NoAccessPath
- If applicable, from the Signal Conditioning list, select a format for mapping the values coming from your process hardware.
- If applicable, from the Hardware Options list, select a device control addressing format for the database block. This selection is overridden if you select a datatype from the Requested Datatype list on the Item Configuration page of the OPC Client I/O driver Power Tool.
For detailed information, refer to the OPC Client Driver online help.