The Event object contains information about event-based events that are monitored by the Scheduler. The Event object will fire a VBA event based on the evaluation of the data source. It can be configured to fire when the value is OnTrue, OnFalse, WhileTrue, WhileFalse, or OnChange.
For more information on the Event object, see the "Scheduler" chapter in the Mastering iFIX manual.
Methods
DoesPropertyHaveTargets Method
GetConnectionInformation Method
GetConnectionParameters Method