The APM_UPDATE_LOGIC webservice manages the temporary tables GE Digital APM uses to load the database. Correct configuration is required for the system to operate correctly.
Open the file to edit, and then configure the following parameters:
Parameter | Description | Default or Recommended Value |
---|---|---|
context | Defines what Talend context environment is used. | Default. Do not change. |
CONFIG_FILE_PATH | The directory path to the context file used for extractions. | C:/APMConnect/Config/ContextFile.xml |
LOG4J_CONFIG_FILE |
The directory path to the log4j.properties file used for extractions. |
C:/APMConnect/Config/log4j.properties |
SAP_CLOUD_ENABLED | Specifies whether the installation is in the cloud or on premises. |
|
Note: All file paths must use / in this configuration as a directory separator or errors will occur.
On your APM Connect server, navigate to <root>\APMConnect\Utilities\runtime\deploy, and then paste the copied file in that location.
Note: If new configuration is not automatically applied, restart the APM_CONTAINER service. This will force the changes to be applied.
Copyright © 2017 General Electric Company. All rights reserved.