The RFC Connector Configuration file identifies the location of the context file and log4j properties file for any client that uses SAP Remote Function Calls (RFC).
Open the file to edit, and then configure the following parameters:
Parameter | Description | Default or Recommended Value |
---|---|---|
context | Defines what Talend context environment is used. | Default. Do not change. |
CONFIG_FILE_PATH | The directory path to the context file used for extractions. | C:/APMConnect/Config/SAP_ContextFile_Client.xml |
LOG4J_CONFIG_FILE |
The directory path to the log4j.properties file used for extractions. |
C:/APMConnect/Utilities/runtime/etc/log4j.properties |
Note: All file paths must use / in this configuration as a directory separator or errors will occur.
Copyright © 2017 General Electric Company. All rights reserved.