Note: To complete the following instructions successfully, you must use SAP client 000.
Steps
If your currently installed ABAP release is 400_600 and level is 0000, and you are not installing the ABAP Add-on in an S/4 Hana SAP system, proceed directly to Step 18. Otherwise, proceed to the next step.
Depending on your SAP environment, navigate to the folder \\SAP Interfaces ABAP Add-On\Service Pack Files\ECC6 or \\SAP Interfaces ABAP Add-On\Service Pack Files\S/4 Hana, and then select one of the following folders:
Log in to the SAP system as a user with:
SCTSIMPSGL and S_CTS_ADMIN authorizations.
-or-
Run the following transaction: SAINT.
The Add-On Installation Tool screen appears.
On the Installation Package menu, then select Load packages, and then select From Application Server.
A message appears, asking if you want to upload OCS packages from the ECS inbox.
Select Yes.
The SAINT: Uploading Packages from the File System screen appears.
Note: In an S/4 Hana environment, 2 files are uploaded and are displayed in the SAINT: Uploading Packages from the File System screen.
Select
.
The Add-On Installation Tool screen appears again.
Select Start.
A new grid appears. MIAPMINT appears in the list of add-on packages that can be installed.
Select the row containing the value MIAPMINT in the first column, and then select Continue.
The Support Package selection tab appears.
Select Continue again.
Notes:
An indicator appears at the bottom of the screen to indicate the installation progress.
When the progress indicator disappears, a message appears, indicating that the add-on package will be installed.
Select
.
The status is updated to indicate that the add-on package will now be imported, and the installation process continues. When the installation process is complete, the status is updated to indicate that the add-on package was imported successfully.
Select Finish.
The MIAPMINT add-on package appears in the list of installed add-on packages on the Add-On Installation Tool screen.
Run the following transaction: SPAM.
The Support Package Manager screen appears.
On the Support Package menu, then select Load Packages, and then select From Application Server.
A message appears, asking if you want to upload the package.
Select Yes.
A summary screen appears, indicating that the package was uploaded successfully.
Select Display/define.
The Component Selection dialog box appears.
.
.On the SPAM: Import: Queue dialogue box, select
.
The import process begins. When it is complete, a message appears, indicating that the import process was successful.
Select Continue.
Another message appears, indicating that the import process was successful.
.On the Support Package menu, select
.
The installation is complete.
What's Next?
Copyright © 2017 General Electric Company. All rights reserved.