Install the SAPCAR File on the APM Connect Server

Note: If you are not using SAPCAR to compress files, then skip this procedure and proceed to the next procedure in the installation workflow.

Steps

  1. On the SAP Server, copy the SAPCAR.exe file.
  2. Access the APM Connect Server.
  3. In the windows system32 directory, paste the SAPCAR.exe file, as shown in the following image:

    The SAPCAR file is installed.

Copyright © 1993-2017 Meridium, Inc. All rights reserved.