This workflow provides the basic, high-level steps for using this module. The steps and links in this workflow do not necessarily reference every possible procedure. For more procedures, see the links in the Related Information section.
Schedule a Job to run in the APM Connect Administration Center.
-or-
Execute a Run-now Job.
Check that the record was transferred into Meridium Enterprise APM.
Note: This step is not necessary to complete the data transfer. However, it is a check to ensure that the transfer was executed successfully.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.