This documentation uses the term Risk Assessment window to refer to the window that displays the Risk Matrix and other risk information, and which can be accessed in various places throughout the Meridium Enterprise APM application. The actual name of the window that appears in the application may be Unmitigated Risk Assessment or Mitigated Risk Assessment, depending on how you accessed the window. Various aspects of the window, including its name, may be customized by an administrative user.
Note: For details on accessing the Risk Assessment window using a particular module, see the documentation for that module.
The following image illustrates what the Risk Assessment window looks like when accessed from an Action in ASM.
The Risk Assessment window contains different items depending upon how you access it. The following table describes the possible items that you might see on the Risk Assessment window.
Item |
Description |
Notes |
---|---|---|
Risk Of section |
Displays the name of the risk. |
An administrative user can modify the label of this section using the Risk Matrix datasheet. |
Unmitigated Risk Rank section |
Displays a value that is calculated based on the sum of
the unmitigated risk values, which are represented by a |
The value in the Unmitigated Risk Rank section is a sum of all of the values on the tabs on the Risk Matrix, multiplied by the appropriate weight and protection level factor (the weight and the protection level factor are configured in Risk Category records and Protection Level records). If the Risk Matrix is configured to use the maximum risk rank, this value is the greatest of all the risk values, not the sum. An administrative user can modify the label of this section using the Risk Matrix datasheet. |
Mitigated By section |
Displays the name of the action or the recommendation that mitigates the risk. |
An administrative user can modify the label of this section using the Risk Matrix datasheet. |
Mitigated Risk Rank section |
Displays a value that is calculated based on the sum of
the mitigated risk values, which are represented by a For a given risk, the mitigated risk rank will be lower than the unmitigated risk rank. |
The value in the Mitigated Risk Rank section is a sum of all of the values on the tabs on the Risk Matrix, multiplied by the appropriate weight and protection level factor (the weight and the protection level factor are configured in Risk Category records and Protection Level records). If the Risk Matrix is configured to use the maximum risk rank, this value is the greatest of all the risk values, not the sum. An administrative user can modify the label of this section using the Risk Matrix datasheet. |
Risk Matrix |
Contains a series of tabs that contain a matrix, where you can make selections that the Meridium Enterprise APM system will use to calculate the overall risk rank. |
For details about the Risk Matrix, see the topic About the Risk Matrix. |
Legend |
Displays the icons that are used to represent mitigated risk values and unmitigated risk values in the matrix. |
None |
Basis for Assessment section |
An explanation of the current risk assessment. |
None |
Save button |
Saves any changes you have made using the Risk Assessment window. |
None |
Cancel button |
Closes the Risk Assessment window, discarding any changes you have made. |
None |
Copyright © 1993-2015 Meridium, Inc. All rights reserved.