Create an Asset Group

Steps

  1. Access the Assets page.
  2. In the left pane, select Group, and then select .

    The New Asset Group workspace appears.

  3. In the Group Name box, enter a name for the new asset group.
  4. In the Group Description box, enter a brief description for the group.
  5. To add a Parent to the Asset Group, above the Add Parents box, select .

    TheAsset Finder window appears.

  6. In the Asset Finder window, use the Asset Hierarchy to select for the level of the hierarchy you want to associate the group with, and then select Done.
  7. Above the Add Assets box, select .
  8. In the Asset Finder window, using either the Asset Hierarchy or a preexisting Asset Group, select for the asset(s) that you want to add to the group, and then select Done.
  9. In the workspace heading, select Save.

    The group is saved, and appears in the Asset Group section.

    Note: Relationships are determined while creating an Asset Group during an associated module workflow.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.