Overview of the Asset Criticality Analysis (ACA) Module

Asset Criticality Analysis (ACA) is a tool that you can use to define the criticality of a system and the individual locations and pieces of equipment that make up that system. The ACA interface lets you define the probability and consequences of the failure events that may occur for a system, which helps you determine which of your systems, locations, and pieces of equipment have the highest risk of failure in your facility. In other words, using an ACA, you can determine which of your systems, locations, and pieces of equipment are critical.

After you have determined which of your systems, locations, and pieces of equipment are critical, you can use Meridium Enterprise APM modules to further analyze and safeguard those systems, locations, and pieces of equipment. For example, through an ACA, you might discover that if Equipment A were to fail, it could cause a catastrophic event in your facility, leading to personal injury. In this case, Equipment A is considered critical, and you may want to use the Asset Strategy Management (ASM) module to develop a strategy for optimizing the performance of Equipment A.

Using ACA, you can:

ACA leverages the standard Meridium Enterprise APM risk matrix that you can use to assess the criticality of your systems, locations, and pieces of equipment. After you have identified the criticality of your systems, locations, and pieces of equipment, you can determine which ones require further safeguarding, analysis, and tracking using Meridium Enterprise APM modules.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.