The queries listed in the following table are provided in the Catalog folder \\Public\Meridium\Modules\Asset Strategy Management\Implementation\Queries. In this table, the values listed in the Query column refer to the query names. The baseline captions are the same as the names.
IMPORTANT: With the exception of the Get SAP ID for Equipment and Get SAP ID for Functional Location queries, you should not modify these queries in any way or move them to another Catalog folder. Also, while modifying the design of the Get SAP ID for Equipment and Get SAP ID for Functional Location queries is allowed, if you are using the baseline Equipment and Functional Location families, it is not necessary.
Query |
Behavior and Usage |
---|---|
Asset Is Equipment |
This query is not used by ASI. |
Get Equipment for SAP ID |
Returns the Equipment record that contains the ID corresponding to the value supplied for the SAP Equipment ID prompt and is linked to the SAP System record identified by the value supplied for the SAP System prompt. In the baseline Meridium Enterprise APM database, the query returns records in the Equipment family. This query is not meant to be run on its own. Instead, the Meridium Enterprise APM system runs this query automatically to determine which Equipment record to link to the new Asset Strategy record when you create an Asset Strategy by importing Maintenance Items, Notifications, or Operations from SAP. When the Meridium Enterprise APM system runs this query, it performs several actions automatically:
If the query returns a record using the provided values, the Meridium Enterprise APM system links that record to the new Asset Strategy record. If the query does not return a record using that value, the Meridium Enterprise APM system runs the Get Functional Location for SAP ID query. Note: Because the documentation for importing SAP
items to create Asset Strategies assumes that you began the workflow by
importing Equipment and Functional Location records using the SAP Interfaces,
this documentation assumes that you will link your Asset Strategy records to
either an Equipment or Functional Location record. You will not, therefore,
need to modify the baseline Get Equipment for SAP ID query to include a
family other than the baseline Equipment family.
|
Get Functional Location for SAP ID |
Returns the Functional Location record that contains the ID corresponding to the value supplied for the SAP Functional Location ID prompt and is linked to the SAP System record identified by the value supplied for the SAP System prompt. In the baseline Meridium Enterprise APM database, the query returns records in the Functional Location family. This query is not meant to be run on its own. Instead, the Meridium Enterprise APM system runs this query automatically to determine which Functional Location record to link to the new Asset Strategy record when you create an Asset Strategy by importing Maintenance Items, Notifications, or Operations from SAP. When the Meridium Enterprise APM system runs this query, it performs several actions automatically:
If the query returns a record using the provided values, the Meridium Enterprise APM system links that record to the new Asset Strategy record. Note: Because the documentation for importing SAP
items to create Asset Strategies assumes that you began the workflow by
importing Equipment and Functional Location records using the SAP Interfaces,
this documentation assumes that you will link your Asset Strategy records to
either an Equipment or Functional Location record. You will not, therefore,
need to modify the baseline Get Functional Location for SAP ID query to
include a family other than the baseline Functional Location family.
|
Get SAP ID for Equipment |
After providing a prompt for an Entity Key, returns the record with the provided Entity Key. In the baseline Meridium Enterprise APM database, the query returns records in the Equipment family. This query is not meant to be run on its own. Instead, Meridium Enterprise APM runs this query automatically to determine whether to populate the Equipment or Functional Location field when you build Notification or Maintenance Item records from Actions. |
Get SAP ID for Functional Location |
After providing a prompt for an Entity Key, returns the record with the provided Entity Key. In the baseline Meridium Enterprise APM database, the query returns records in the Functional Location family. This query is not meant to be run on its own. Instead, it is run automatically to determine whether to populate the Equipment or Functional Location field when you build Notification or Maintenance Item records from Actions. |
Locate Packages for Navigation |
Returns all existing the Implementation Packages that contain one or more of the Asset Strategies that belong to the current Implementation Package. This query is not meant to be run on its own. Instead, it is run automatically when you select the Navigate link on the Packaging page. |
Locate Strategies to Package |
Returns a list of Active Asset Strategy records that are not linked to an Implementation Package record. This results of this query are displayed on the Select Asset Strategy to Add to Package window, which you can access via the Implementation Package Update page. You can add criteria to this query, but you should not remove any criteria from the query. |
Locate_Packages |
After providing a prompt for State and Implementation Role, returns a list of all Implementation Package records that meet the specified criteria. This query is run when you select the Packaging link on the Asset Strategy Implementation Overview Page. |
Locate_Packages_for_Execution |
This query is not used by ASI. |
Locate_Packages_for_System_Strategy |
Returns a list of all Implementation Package records that are linked to the Asset Strategy record to which a given System Strategy record is linked. This query is run when you select the Strategy Implementation link on the Navigation menu when you are viewing a System Strategy. |
Locate_Packages_for_Unit_Strategy |
Returns a list of all Implementation Package records that are linked to the Asset Strategy record that is linked to the System Strategy record to which a given Unit Strategy record is linked. This query is run when you select the Strategy Implementation link on the Navigation menu when you are viewing a Unit Strategy. |
Move to Existing Secondary Package |
After providing a prompt for an SAP system, returns all existing Implementation Packages associated with the selected SAP system, except for the current Implementation Package. This query is not meant to be run on its own. Instead, it is run automatically when you send an Action to a new or existing Implementation Package. |
Copyright © 1993-2015 Meridium, Inc. All rights reserved.