Recommendation Management is a tool that allows you to define and to record the method by which risks are identified and mitigated in the form of Recommendations. Once an analysis is completed, Recommendations can be managed through the Recommendation pane. After Recommendations are successfully managed, the consolidated collection of Recommendations are promoted to Actions.
You can access Recommendation Management from the Failure Effect workspace of an RCM or FMEA analysis, as detailed in the Access Recommendations in RCM topic.
See the Recommendation Management section of the documentation for additional options when working with recommendations with RCM and FMEA analyses.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.