About Full Processing and Incremental Processing

When you process a cube on the Analysis Server, either manually or using a schedule, you have the option of choosing full processing or incremental processing.

Note that when full processing is performed, Metric Views will become inaccessible to users who are currently logged in to the Meridium Enterprise APM and have already accessed the Views. Users will need to restart the Meridium Enterprise APM application to access Views after a cube has been processed using full processing, if they are logged in at the time the processing occurred. Meridium Enterprise APM does not need to be restarted when incremental processing is used.

Therefore, if you are scheduling cubes for processing and need to use the full processing option, you should schedule the processing so that it occurs at a time when users are not using the Meridium Enterprise APM system. If you are scheduling cubes that are unlikely to change, you can use incremental processing and schedule the processing to occur at any time.

 

Copyright © 1993-2015 Meridium, Inc. All rights reserved.